I think that my bluetooth cc256xqfnem is damage because the movil cel doesn't detect it.
i have connected pins like the CC256x Testing Guide says but it doesn't respons
RF1 connector ( PIN1 and pin 19 to GND), (Pin 5 with 1.8 V ),
RF2 connector (PIN 7 and 9 with 3.5 V) and (PIN 19 with 0 votls )
What can i do?
I'm using a launch pad msp430G2452IN20 too