Hello,
I'm trying to use Bluetooth Hardware Evaluation tool v1.0 for RF performance testing. I don't have the evaluation board msp430 but I used the follow information to do my setup:
"The other way it can be interfaced is that the PC is directly connected to the HCI interface of the CC256x device without the CPU/MPU present. This can be done using a USB/Serial converter to translate the USB voltage levels from the PC to the Serial voltages of the CC256x device"
This allowed me to send HCI commands through TX and see the response from bluetooth module using HCI tester, so the communication is working well.
The problem is that i tried to use the Bluetooth Hardware Evaluation Tool V1.0 to load Service Pack into bluetooth device but i always get the error: "Com Port Timeout”.
It seems that the Bluetooth Hardware Evaluation Tool didn’t use hardware flow control.
When I checked PC RTS line, signal was always high.
Could you check for this?
Waiting for response.
Thank you.