This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PAN1326B(CC2564B) SP 1.0_BT_Spec_4.1.bts with Bluetopia Stack

Hi,

I am using Bluetopia 1.4R2 in which CC2564B.h contains a patch labeled SP 0.2 which works just fine initializing the chipset.

I then visited the wiki and download the latest patch for CC2564B, used the BHET tool, loaded the file, saved it as .h format, modified it from byte data to 16bit word data and then used it to initialize the chip - it does not work, however if I revert to the SP0.2 patch in the code, it works fine. I have attached the file - please let me know why it wont load properly.

7345.Untitled.h

Ron