Hi,
MSP430 New release v1.5 R1 is now available.
New Demos And Applications:
- PXPDemo
- FMPDemo
- Modified A3DPDemo_SNK - A3DPDemo_SNK has been modified to allow up to two incoming A2DP sources. When a new source connects in, or an existing source attempts to start streaming audio, any currently-playing streams will be paused
- A3DPMultiRoomDemo -- This application shows how to utilize the A2DP function of the Bluetopia core stack and the Assisted A2DP (A3DP) of the TI CC2564. This will act as a Sink device, demonstrates the AVRCP Controller core, and includes an updated service pack for the CC2564 that allows for a special “Multi-Room” vendor-specific command to forward an existing A2DP stream to a secondary speaker running the same service pack on another CC2564.
CC256x MSP430 Bluetopia Basic Demo APPS Wiki : http://processors.wiki.ti.com/index.php/CC256x_MSP430_Bluetopia_Basic_Demo_APPS
Tiva C New release v1.2 is now available.
New Demos And Applications :
- A2DP Demo
- A3DP Demo SNK
- A3DP Demo SRC
- A3DP MultiRoom Demo
- HFP Demo
- HOGP Demo
- MAP Demo
- PBAP Demo
- Added TIRTOS support for SPP and SPPLE Demo
CC256x TIVA Bluetopia Basic Demo APPS Wiki : http://processors.wiki.ti.com/index.php/Stellaris_Bluetopia_Basic_Demo_APPS