Hi,
Please go through my understandings and problems I face below and provide clarifications:
1) I chose CC2564B to implement dual mode bluetooth functionality in my product. '2564B' particularly because it is a dual mode chip and supports assisted A2DP profile. I need audio sourcing in my product and hence A2DP profile is mandatory.
2) The module available with integrated CC2564B is PAN1326B from Panasonic.
3) For developing a prototype for my product, I need an evaluation board containing PAN1326B module because only PAN1326B contain CC2564B which support A2DP profile.
Qn1: Which evaluation board can I choose?
Note: I found PAN1323-ETU which doesnt contain CC2654B.
4) I should interface an MCU with PAN1326B in my product, and hence for prototyping I require another evaluation board which contain that MCU. MSP-EXP430F5438 experimenter board containing MSP430F5438A seems OK for me.
Qn2: Is SDK support with assisted A2DP profile available for MSP430F5438A MCU?