Hello,
We have the development board TIVA C TM4C123G with the bluetooth Evaluation Module cc256xQFN-EM. We loaded the SPPDemo code and it works perfect.
We copied the same hardware for our custom design using the TM4C1230H6PM controller with CC2654B BLE chip.
We are getting BTPS_ERROR_HCI_INITIALIZATION_ERROR -4 error while execution the "OpenStack()"
I can confirm that the BLE device indicates that the power-up sequence is complete as BLE RTS goes low. But after about 6secs when this error message "Stack Init Failed: -4. Unable to open the stack." gets printed on console the BLE RTS and nSHUT go HIGH again.
Also I can see some data on the controller Tx line. But Controller RTS is not low when controller transmits data. I am also not sure of the TM4C1230H6PM controller is able to read the BLE RTS either.
Do i need to make some more change in the code to be able to port it successfully on TM4C1230H6PM controller? ( All i changed is the device name in settings/options menu in Keil Compiler)
Thanks,
Vahbiz