Hello,
We are using the EK-TM4C1294XL development board with the TM4C1294ncpdt processor and the PAN1323ETU board to connect to another device using Bluetooth LE via the Bluetopia SDK. We are running into an issue with the call to BSC_Initialize(), where the FaultISR is being called after a few seconds.
We can breakpoint on the execution of HCITR_COMOpen and HCITR_COMWrite, and both seem to execute normally. However, when we break on the execution of HCITR_COMClose, we are receiving an HCITransportID which is invalid (~168,821 instead of the expected '1', and the received value changes every execution). After this function is called, we enter the FaultISR.
We have also tried using the __SUPPORT_CC256XB_PATCH__ flag, as I am unsure if it is using the CC256x or the CC256xB part, but having or not having that flag does not change the operation.
We are using CCS v6.0.1 and Bluetopia's M4 v1.2 stack.
Thank you,
- Glenn