Hi all,
We are using an MSP430F5438 and CC256x to talk BLE to iOS, WinPhone and Android devices. If an android or winphone device is connected I can call GAP_Query_Remote_Device_Name() and it returns the correct device name whether connected via BLE or BDR.
However, if I make that call to an iOS device via BLE I only receive a single character back, a '*'. I have tried with 2 iphones and an ipod. We don't have MFI so I cannot connect via BDR and see if the result is the same. Is there some other way to get the device name in BLE in the bluetopia stack?
Regards,
Barak