Hi,
I am sorry if I duplicating an issue from previous posts by me.
but again, I need a help!
all what I need is to develop FW for a device, the device will be a slave that make pairing by SSP (secure simple pairing) with an application running on smartphone.
after pairing, upon a packet from the application, I need to forward this packet by UART to a PC, then the PC will return a packet that I have to transmit it back to the application.
so I need to keep connected by BT to a smartphone and by UART to a PC all the time without aborting.
(a previous version of a project was a direct UART communication between two devices, now I have develop a device as adapter BT/UART...)
I need a help by choosing the right hardware (Evaluation board, Microprocessor, BT chip...) and the software example that I need for my device.
just I started with BT-MSPAUDSINK & CC256x MSP430 Bluetopia SDK.
can I get what I want by this board? if yes so which software example can I base on and which changes I have to do?
if no so which hardware & software I can use to achieve my aim?
Thanks.