Hi,
We have our system built based on Tiva-C series running TI RTOS and CC2464B with Bluetopia SDK V1.2.
We are trying to implement low power mode and use Sleep Call back event from CC2564. We are trying to use CTS line as one of the wake-up line and we are failing.
We see that, once CTS line is asserted, it is not de-asserted when Bluetopia Stack indicates safe for entering sleep mode through call back function.
We are using COM configuration as indicated in reference code.
HCI_DRIVER_SET_COMM_INFORMATION(&HCI_DriverInformation, 1, VENDOR_BAUD_RATE, cpHCILL_RTS_CTS);
Question from me:
- What is the expected behavior of CTS line? Will CTS line de-assert when
- Are there any special HCI commands to be issued for the BT Chip to be low power mode?
- Should we need to execute any special VS commands for making this work.
Please help me in clarifying the doubts.
Thanks in advance,
Best regards,
Gupta