Dear All,
We have used PAN1326 BT module with MSP430F5438A. We are using Stonestreet One SPP Bluetopia stack. PAN1326 BT module is not responding midway while downloading the Patch to the PAN1326 module. HCI_Send_Raw_Command returning -14 errror( BTPS_ERROR_HCI_DRIVER_ERROR) and then HCITR_COMClose function getting called and it shutdown the PAN1326 BT module.
I have verified PAN1326 BT module using CC256x Bluettoth Hardware evaluation tool to load the Bluettooth service pack bluetooth_init_cc2564_2.12.bts into PAN1326 successfully, and verified all the RF testing mode successfully. I have checked the UART interface With sniffer to monitor both Rx & Tx line. We came to know that The PAN 1326 module hasnot responded to the last send command by the microcontroller to the PAN1326. The UART interface is propper.
We are facing this issue with 4 devices out of 20 devices. I am not understanding what the issue is.
Please reply me ASAP. Thanks in advance.
Regards,
Bhairu