Hello,
I'm working with CC2564 directly with HCI_Commands from an AVR xmega (without BLE Stack) and I do not succeed to make it a discoverable peripheral.
I've also noticed that the structure of the received events is not the same as I found in some posts.
This is the log containing the commands that I send and the events that I receive.
reset
-----------
TX: 01 03 0C 00
Rx: 04 0E 04 01 03 0C
get_local_version
-----------------------
TX: 01 01 10 00
RX: 04 0E 0C 01 01 10 06 06 0D 0F 1B
read_bd_address
-----------------------
TX: 01 09 10 00
RX: 04 0E 0A 01 09 10 F3 D3 5E E9 17
le_enable
-----------
TX: 01 5B FD 02 01 01
RX: 04 0E 04 01 5B FD
init_as_peripheral
------------------------
TX: 01 00 FE 26 04 05 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01 00 00 00
RX: 04 0E 04 01 FE 02
update_advertising
--------------------------
TX: 01 07 FE 05 01 03 02 01 06
RX: 04 0E 04 01 07 FE 01
make discoverable
--------------------------
TX: 01 06 FE 0F 04 00 00 00 00 00 00 00 07 00 00 00 00 00
RX: no answer received
Please advise !
Thank you in advance and best regards to all community,
Sorin Leibovici