All:
Hi,I use two (msp430f5438a + cc2564b) to developing some application , the referense code is v1.5r2 of bluetopia for msp430 .
I want to construct relations between server and client by using gatt and gap .
there are two side or role : cc2564_roleA ,cc2564_roleB .
there are two Characteristics:
one side: Write Characteristic using for cc2564_roleA send infomation or command to ble device cc2564_roleB.
( BLE Properties: Write , Date Type: Byte[] ,Date Length: 20 )
another side: Notify Characteristic using for ble device cc2564_roleB send notify infomation or command to cc2564_roleA
the problem is :
GATT_Initialize , GATT_Register_Service is using for Gatt Server initiate ,
How can I Initiate a Gatt Client to relate to Gatt Server ?