Hi all,
We have used PAN 1326B module for our hand held design. The proceSsor used is the MSP430. Out of three boards which we have assembled, two are showing a Bluetooth range of a little over 10m LOS, enabling our hand held device to connect to the base unit (similar to a tablet). However, in one of our assembled boards the range is lesser than 5m after which the hand held device is disconnecting from the base unit.
What can be the possible reasons why this can happen?
Regards,
Athira