Hi,
Question 1:
I am using cc256x module and I am using multiple spp comports. At first I connect to connect to "Port 1" and role is happening properly and this comport connection is still occupied with the same device.
If I use another device to connect on "port 2" then also I am observing that cc256x is changing it's role to master again.
Is it a case that for each SPP port there should be a role change event???
Question 2:
When comport 1 is connected to one andriod(phone) device and with the same andriod device(phone) when I try to connect a completely different device which is also a salve , then the observation is andriod device (phone) is changing to master and then again it is changing to slave. Thus CC256x com1 is changing it's role from master to slave. Thus this effect the role change of another comport say "Port 2 of CC256x".
Question 3:
As a slave to how many devices that cc256x can connect ?? 7 is possible . I am unable to connect more than 2 master devices. core spec says that salve can participate in multiple piconet.
Question 4:
Once device is master can I stop changing it's role ??
Thank you