Hi,
I search on the forum before to post, but I found nothing clear about this issue, and it looks like I am not the only one with this need.
I am at the edge of a project based on MSP430 and CC2564b. I am using the HFP demo as a basis.
The thing is that I need to enter the passkey and initiate the process with my smartphone each time I want to connect it with my Bluetooth device.
My goal is to make it autoconnect with the receiver already paired when the code start. i.e. After starting I check if the known host is in range and connect it if possible.
Is a function like that implemented in Bluetopia? Do you have at least a code example to implement in my project? Or even a guideline to proceed?
I am using BLuetopia stack for MSP+CC2564b v1.5R2.
Thank you in advance,
Best regards
Anthony