Hi ,
We are able to start the TiWi-uB2 with MSP430F5438A Experiment board. Initially it was giving problem (i think due to CTS line)
When we have enabled the Pull-up for the CTS line in code the Stack Initialization Error :-4 removed and able to access Bluetooth.
But right now we have strange problem with SPPDemo example code..
We are performing : Example connection using Blueterm
When we are sending the Pairing request from the Android phone , we are not able to get PinCode request and etc as given on the above link
Also after sometime - Both LEDs on the MS430-Expreimenter board blinks at slow rate.
Also we have found Inquiry command is not working properly. We are able to Run the demo but not successfully.
If possible kindly let us know what will be the issue.. (Is CTS - Required Pull-up enabled.. without this we are not able to run the code..).
and LEDs blinking at faster rate.