Hi,
i am trying to get an answer for a Sync Message i send via HTERM to a CC2564MODNEM Bluetooth Controller. Between my PC and the CC2564 i connected a SEGGER j-link EDU and a board with UART. I want to use the UART Three-Wire connection. I checked with an oscilloscope if the signal arrives at the Debug Pin 12 (HCI_RX with 1.8 V). It arrives and it has 1.8 V.
I created the header and sent a 0x01 and 0x7E afterwards as it stands in the Volume 4 HCI Transport specification of Bluetooth in Part D under point 8.4 (packet type 15, unreliable message, payload length 2). The Controller should send back 0x02 and 0x7D, but it doesn't. I use a 115200 baud rate. What do i do wrong? What is the correct header for the Sync Message?
Regards and thanks in forward
Max