Hi,
I meet a question when initializing CC2564. A MSP430 connects to CC2564MODNEM board running with Stonestreet One Bluetopia stack. The stack reports an error as below,
Stack Init Failed:-4
Unable to open the stack.
I measure the shutdown pin from MSP430, the HCI_RTS pin from CC2564, 32.768k clock on CC2564 board, 3.3V and 1.8V power, according to the initialization requirements. The clock and powers are all correct. But when the shutdown signal change from low to high level, the HCI_RTS does not turn to low level, it keeps high.
Why CC2564 HCI_RTS not respond? Hope your answer. Thanks.