CC2564 Champs,
We are using the bluetopia API VS_Set_Max_Output_Power to set the max power. This in turn calls VS commands 0xFD82 and 0xFD87. Will this have any effect on BLE power?
I see that setting the power vector will change power for GFSK but it looks like this may only be for basic rate and not for LE.
On the wiki page: http://processors.wiki.ti.com/index.php/CC256x_VS_HCI_Commands#HCI_VS_DRPb_Set_Power_Vector_.280xFD82.29
It says “NOTE: Power level 1 is used for BLE power”. To change BLE power do we need to use command 0xFDDD?
HCI_VS_DRPb_Set_Class2_Single_Power (0xFD87) --> Is this used to set the power of another device? Not the DUT.
HCI_VS_DRPb_Set_Power_Vector (0xFD82) --> Does this set available power levels (1-15) for ONLY BT Classic’s Basic Data Rate(GFSK), EDR2, EDR3? Or does it also effect the GFSK used by BLE? What are the effects of modifying the power level 1?
HCI_VS_LE_Output_Power (0xFDDD) --> Used to set current power state for BLE. Does this reference the Power Vector set by 0xFD82 for GFSK? It is unclear how Power Level 1 applies here.
The root of my question is, will commands 0xFD82 and 0xFD87 have any effect on BLE output power? It is unclear how these commands intermingle, can you please clarify them.
Thanks,