I would like to use the SS1 HID Demo as a starting point to implement a custom bluetooth (classic) HID device and I'm having trouble finding how to set device information such as VID, PID, SerialNumber, etc. (to be used for device enumeration)
I'm using a BT-MSPAUDSOURCE-RD (MSP430F5229+CC2564B) with the CC256x MSP430 Bluetopia SDK v1.5 R2. I've modified the sample HID Demo to work with the BT-MSPAUDSOURCE-RD and have been able to successfully pair and connect to the device from a Windows 7 machine. However, when I look at the hardwareID of the HID compliant mouse, there is no VID or PID, just the generic: HID\{00001124-0000-1000-8000-00805f9b34fb}_LOCALMFG&000a (please see below).
I have looked into using the DIS api, but that seems to be for GATT and BLE devices - is this correct?
Can someone please help point me in the right direction for setting this information?
Thank you in advance!
Chris.