I am using the TI Bluetooth stack with PAN1326B module. We are not using the Bluetooth Low Energy (LE) and the Deep Sleep mode associated with LE. We would like to implement a mode called IDLE when the Bluetooth is still active but working at a lower clock. We also will reduce the clock frequency all host MCU clocks to reduce power. I have couple of questions:
1. How can I ensure that changing the MCU clock will not cause an error in Bluetooth operation.
2. Can I suspend the UART without going to Deep Sleep mode without breaking the synchronization between the host and the base band.
3. Is the command HCITR_COMSuspend(unsigned int HCITransportID) only works with LE .