Hello
I'm trying to modify the firmware trf7960evm to add iclass protocol.
Looking and reading the forum I found an answer I do Josh Wyatt where he directed another person by sending a PDF on "interoperability trf796x_v2."
In that file there was a presentation of how to approach the configuration of trf and command uses this protocol.
Try to follow this guide and I found several problems that surely you will be able to answer.
The file sets the ISO Control to "0x86" which is ISO15693 hight rate 1 out 4 FSK.
But according to the datasheet I could get from 2k PicoPass
the modulation amplitude does not the frequency, then no would have to select the 0x82?
Another rarely found in the file is that when a weapon PicoPass command such as ACTALL
the 4 bits are misconfigured more weight compared to the datasheet (more precisely the M1 and M0 bits are reversed)
The tests could take, even with these doubts gave me these results.
Sending a command ACTALL detect because the card seems to return something but in the registration of irq always detect collision and framing error.
I would like your opinion or if I'm wrong.
From already thank you very much to all for the help forum and also to Josh Wyatt for all the answers it gives.