Hi,
I am hoping someone can help me with my TRF7970A design. I can't find anywhere in the datasheet where it mentions the maximum digital input voltage.
The VDDIO pin can be used to set the digital output voltage range and input VIH and VIL thresholds proportional to VDDIO.
In my design the TRF7970A powers VDDIO from its VDDX output, derived from the 5V VIN supply.
My microcontroller is powered from a seperate supply at 3.3V and can take up to 5.5V on its inputs unpowered, so if the TRF7970A was to assert an output before the microcontroller supply is up then it is ok.
Going the other way, if the microcontroller were to assert a logic high before VDDX comes up I need to make sure the TRF7970A input will survive.
Do the TRF7970A inputs have input clamp diodes to VDDIO? Can they tolerate in input voltage independent of VDDIO or does VDDIO need to be up before any signals are applied?
For some reason I can't seem to find the input voltage range in the datasheet, just the high/low threshold voltages. Also VIH is listed as a max which seems a mistake as usually VIH threshold is listed in the MIN column, i.e. to be logic high the threshold needs to be 0.8VDD minimum.
Thanks in advance, Mark