Hello E2E community,
We have released a robust Peer to Peer reference design supporting both active and passive P2P at 106kbps, 212kbps and 424kbps. The CCS project has support for both the MSP430F5529 Experimenters and Launchpad boards ( see below for more information on how to choose which board to download the code). The demo has two modes (Standalone mode and a GUI mode) which help simplify the testing mechanism with existing NFC enabled platforms by enabling the desired NFC P2P mode. Furthermore, we have completed extensive testing with the most commonly used NFC enabled handsets, including throughput performance and interoperability testing.
When the CCS project is downloaded and imported inside Code Composer Studio, there will be two possible configurations to choose the target board (as shown below ) :
Build Configurations ==> Set Active ==> MSP430F5529_EXP_BOARD or MSP430F5529_LAUNCHPAD
For more information about the firmware and software please visit : http://www.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=sloa192
Best regards,
Erick M.