Hello, I reference sloc132 design has a based on TRF7970A of high power circuit board, using TI provides of source program (sloc300a), and according to TRF7970A of DATASHEET description set the register 0x0B of BIT6 and 0x09 of BIT3 to 1。using spectrum analyzer observation output power has reached 4W, antenna using 50*30CM of high performance antenna, but reads the tag of ISO15693 of effect is is poor, only several CM, Could you tell me how it should be configured in order to improve performance (>50CM). Could you give the program of the designed sloc132 ?
Thanks,
Regards,
Bob