I am trying to get the kit up and running according to the instructions at http://www.ti.com/lit/ml/slab069/slab069.pdf.
1) When I complete the step "Load the Target Binary" i do not get a heartbeat until I close UniFlash.
2) As soon as I open the Stollmann NFCPlayer (version 1.0.57.5) the heartbeat LED turns off (stops blinking).
3) After selecting Start NFC I get NFC: Start Fail in the lower left corner and the log reports
! CNfcInstance::nfcStart:Creating a RW-NFC-instance failed (code:4)
! CNfcPlayer::nfcStart:Instance initialization failed (code:4)