I am developping a NFC card reader board, but it is not clear for me, what is the ISO standard to comply to for my application, could any one teach me about that?
NFC ISO Standard that I found:
ISO 18000-3
ISO 18092
ISO 15693
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am developping a NFC card reader board, but it is not clear for me, what is the ISO standard to comply to for my application, could any one teach me about that?
NFC ISO Standard that I found:
ISO 18000-3
ISO 18092
ISO 15693
Hi Gianluca,
Depending on the tags you are trying to read there are a number of ISO specifications to investigate:
Type 2: ISO 14443
Type 4A/B: ISO 14443, ISO 7816-4
Type V: ISO 15693
There are also additional NFC specifications (which include information on Type 3 tags) available from the NFC forum. You can register on the NFC forums official site to download those.
If you are interested in further details about Type 3 (FeliCa) tags as well, those documents come from Sony.
Thank you Ralph, my goal is to develop one electronic board able to read NFC TAG of the cellular phone.
Which ISO standard do normally they employ?
if you are wanting to read emulated card in the cell phone, they use ISO14443A and ISO14443B (they switch between the two)
not really NFC...more RFID and ISO7816-4, even though NFC is the "buzzword" these days.
and here attached is an overview of the ISO standards and NFC specs and how they are related.