Does any one teach me if ISO 14443A/B compliant device, as TRF7960, can read ISO 14333A compliant devices, as thouse implemente inside Hotel wristband?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gianluca -
the TRF7960, -60A, -63A, -64A and TRF7970A can all read ISO14443A compliant and ISO14443A air interface and -3 standard compliant devices.
Examples of fully compliant device would be Mifare DESFire EV1,
Examples of air interface and -3 (but not -4) compliant devices would be: Mifare Classic, Mifare Ultralight, Ultralight C
To my knowledge all of these are widely used in the hospitality industry.