Hi,
One of our customer is using TRF7970A in their custom board.
And they have below issue in Read/Write mode.
Out of 17 boards 1 board has a problem with some commands(Mifere WUPA)
The issue is DATA in FIFO is ZERO even if the RX is completed succesfully.
Below is the procedure.
1.The TRFxx starts RF modulation.
2.The TAG replies
3.TRFxx generates IRQ after the completion of TAG's response.
4.But the Data size is Zero in the TRFxx FIFO Status ..
Which means TRF7060A has sent a command to the TAG and
the TAG has replied back(with IRQ generated) but the FIFO is empty.
Once this issue occurs TRFxx can only be recovered to normal operation
only after a power cycle.
Please let us know if there is any idea or suggestions about such issue.
Best Regards
Kummi.