Hello,
We are starting a project where we wil use the rf430cl330h as a dynamic tag and after reading all the datasheet there is an unresolved qüestion for me: I don't find a way to protect the device from an external writing (NFC interface) once the memory is written.
In the datasheet it explains that the content can be protected through access conditions in the capability container of the tag. I understand that this means that the write protection is set inside the NDEF frame.
But, what happens if someone tries to erase the content of the memory through NFC without using NDEF format? Is it possible to write directly to the memory of the rf430cl330h using NFC without following the NDEF format? If this is possible it seems that no security protection against erase or write can't be performed. Is this assumption correct?
Same qüestions in a more direct manner:
- Is it compulsory to write to the memory using NDEF format ?
- Is it possible to perform a direct write?
This qüestions should be answered always taking into account a NFC access, I know that this can be done through the I2C interface without any problem, but our concern is related to external access through NFC and how to protect it.
Thanks in advance for your answer,
Víctor