Hi,
How long does it takes to wake microcontroller up from 3D LF reader in the worst case?
I mean absolute time (ms) for Wakeburst + SOF + Wake Pattern (24 bit) + EOF
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
How long does it takes to wake microcontroller up from 3D LF reader in the worst case?
I mean absolute time (ms) for Wakeburst + SOF + Wake Pattern (24 bit) + EOF
Dear Josh,
I look through datasheet but can't compose real timing based on a lot of graphics and tables. I do not understand this technology thoroughly, but just want to evaluate if it suitable moving railway container identifying. So I need to understand minimum-maximum (or typical/recommended) time needed for 3D Wake up process. It’s not a problem to calculate timing for sending 433 MHz RF packet, but 3D LF packet is hard to understand.
I see some real figures for bit timing (table Table 24-19) but how many bits will include full wake-up sequence from t_wake till EOF?