Hi,
Since I flashed the newest firmware from the download section (sloc300) into the TRF7970A I can't connect to the target with the GUI (SLOC301). I get a timeout error when the gui tries to connect. Also with other tools like HTerm I do not get any responds. I also tried the lagency firmware (SLOC250) with the same error. Do I'm using the wrong firmware for working with the GUI?
Thanks for help.