A medical scientist informed me that a blood sugar measurement system (adhesive patch sensor) repeatedly gets destroyed when he passes admission controls for ski-lifts. He asked me for help on that problem. I would like to ask if anyone knows about such issues associated with the RF430FRL152 chip.
The battery powered sensor uses the RF430RFL152 chip for wireless communication (printed antenna with approx. 25mm diameter). The skiing admission systems operate, such as the RF430, at 13.56MHz. They also use passive ISO 15693 cards. Obviously the RF430 is not tolerant against the magnetic field strengths of the lift system. In the chip datasheet there is no information about the protection of the antenna pins. Is there any kind of suppression element implemented? I assume that these lift systems use powers increased beyond ISO standard for higher people throughput.
Is it possible that high H-fields destroy the chip, or is there plenty of headroom? The manufactures of the blood sugar sensor know about this issue, but there were unable to do anything against it. So if the antenna pins were too sensitive, would it make sense to put a suppressor diode on the antenna, or to cover the sensor for skiing with aluminium foil of a few skin-depths (approx 0.1mm) for RF shielding?
Is there anyone who also experienced damage due to other 13.56MHz RFID systems, or knows something about how to fix this problem.
Best regards
Thomas