Hi everybody,
I have no problem to program my RF430FRL152H with the firmware found on TI website (Default, NFC or SensorHub).
What I want is to program it using my own code, and still have the RF stack working with the TRF7970A.
To be simple, I would like to drive pin P1.0 and pin P1.1.
These pins are driving two LEDs, and ADC0 is used to convert the result from a photodiode.
To drive these pins, I would like to use my own two RF commands, same as Read Block or Inventory request.
If I'm right, I have to patch these new commands to be understand by RF430FRL152H ROM code.
Do I have to take example of SensorHub project to patch new RF commands ?
In this example, functions declared are automatically called by the ROM code, once their turn is up.
I don't want it to be automatically, I want the TRF7970A to be the master for calling these new RF commands.
Any idea ?
Florent.