The TRF7960 reader's output can either be 8 ohms or 4 ohms depending on the input voltage. Should the matching components be changed when switching from 5 volts to 3.3 volts? I can only find literature on the 4 ohm output match. I'm running it at 3.3 volts so I matched the output to 8 ohms. I would think that if the reader was operating from 3.3 volts with an 8 ohm output the match would have to be changed for maximum efficiency.
Also, I've designed an external class e amp and everything looks good except the voltage that would be at RX1 and RX2 is in excess of 3.3 volts. It's roughly 5-6 volts. I'm planning to attenuate the signal, but I want to know if the RX1_in and RX_2 in pins have protection diodes.
Thank You