Hi,
First of all, I'm new to NFC..
Second, I would like to test the feasibility of the following, please advise-
The general application works inside industrial environment at 2.4GHz using CC3200- when a controller is control number of base stations (controller and base station with CC3200).
Each base station must get its station ID (1,2,3 etc..). sometimes it will be needed to change a base station and a station ID will must be inserted to a new base station (e.g. base station No. 4 is not working, so it is replaced by a new base station which must get ID No. 4).
My question is- could this be done using TRF7970A Reader (for example) inside the base station and proximate bar code patch on a near by pole (approx. 5 cm)?The ID will be already "stamped" on the bar code, the new base station will be installed and powered and the NFC reader will read the ID and send it via SPI to the CC3200 MCU- is it possible?
THANKS!
Ram