Hi,
I have a requirement to control the RF output power for this device
when running an RFCOMM/SPP profile for both BR/EDR and BLE. I have the
HCI vendor-specific user's guide
http://www.digitalsignallabs.com/hci-vs-commands.pdf
and I am trying to determine which of three RF power commands is the
right one to use.
1. Section 6.1.67 defines a "DRPb" "class 2" RF power command. I
don't know what DRPb means or what "class 2" is.
2. Section 6.1.73 defines another "DRPb" RF power command.
3. Section 6.1.103 defines a "FE" configuration command. What is
"FE"? The field "MAX Allowed output power" seems like it could be
the control I want, but it does state that this sets the "maximum
output power." I don't really want to set the maximum power level,
rather, THE (unvarying) power level.
I would appreciate any clarification on how we can set RF power level
for the WL1271L device.
--Randy