Hello,
I am using CC3000 for scanning APs, I have some questions regarding the wlan_ioctl_get_scan_results function.
1. Is there anyway that make the entries returned based on BSSID instead of SSID? Just like wifi analyser in cellphone. I found that each result table only return one entry if there are more than one AP under one SSID, and returned randomly.
2. Can I send the updated scanning result right after scanning? Flag status of the scan is always 1 which means the result is not aged result. However, now seems it always send the old data even I set the aiIntervalList to be a low value(50). Whats the difference between The status of the scan and isValid in the scan result table?
3. I want to use Tiva C Series LaunchPad to replace the FR5739 which I am using now. In the SDK, there is some code for LM4F120, are they the same board or not? Can I use the code for Tiva C Series LaunchPad?
Thanks and regards,
Zheng