Newbie here. I've been using the getting_started_with_wlan sample code and an MSP430 Launchpad to do some preliminary playing around with the CC3100.
It looks like this code uses a UART to let the MSP430 communicate with the CC3100. In our final implementation though, we will most likely be using SPI. Can anyone tell me how to modify these routines such that SPI is used instead of a UART? I couldn't figure out where either SPI or UART is specified in the code.