Hi, i am working with a f5529 launchpad + CC3000BOOST. I changed the ports from the example in CC3000 SDK1.12 for the ports of the launchpad, as the default version uses the experimenter board. All of this worked fine a month ago. But now, i am unable to configure the IP correctly. I run the smartconfig (command 01), no problem, i get "Smart config DONE\rDONE\r". Then i send the ip config command (command 08), with the good arguments: 08c0a80170c0a80101 and i get "DONE\r". But i dont receive anythin when pinging on IP 192.168.1.112 or whatever IP i choose. There must be something i used to do correctly since it worked before but now it doesn't :S