Hi,
I have a board MSP430f5438a on which there is a intergrated cc3000 TIWI-SL Module.
The connection of WLAN is ok. The sending of data from cc3000 to my PC is ok too (UDP).
But, when i try receiving data from PC, the program goes always into a non-end LOOP.
when i call the fucntion revfrom(), then the program goes into event_handler.
After i send a data to CC3000, the program goes into "HCI_EVENT_REVFROM" , that is right. But, there is a "IF"
statement :
if(((tBsdReadReturnParams *)pRetParams)->iNumberOfBytes == ERROR_SOCKET_INACTIVE)
then program gose into it, and execute the statement :
set_socket_active_status(((tBsdReadReturnParams *)pRetParams)->iSocketDescriptor,
SOCKET_STATUS_INACTIVE);
is that right?
Because i use an old patch programmer(but it is already the newest.), i dont know if something wrong with my SPI or something. My driver version is : 1.6.1.2 , but at least the sending of data is fine.
is there anybody met this problem ?
Thanks for giving me some suggestions.
Best Regards,
Shaguar