Hi,
It is said in the data sheet that Additional testing maybe required for Host end product type.
Class A and Class B testing is Needed in the Host End Product.
1) Please conform me what type of test Covered in the Class A and Class B?
Wifi processor doesn't work directly to comply 30W Eirp. It needs a Front end module and filter. The following information we are looking from TI.
2) In the Block diagram of the CC3000 there is a front end module.It consists of LNA+PA and switch. Is there any recommendations for Switch,PA and LNA modules from TI. If it's not there we need to get the following info from TI.
3) Is there any system level calculations to share. Example : System Noise Figure,Phase noise calculations,noise power levels etc. Any relevant information related to chip. Please provide.
4) To make a final Wifi Radio what digital Peripherals need to be added to CC3000.
5) More briefly 3rd Point, Is there any Ethernet processor for router and Memory stacks ICs need to be added.
Rgds,
Uma Mahesh