My CC3000 is no longer responding to any commands besides the HCI_CMND_SIMPLE_LINK_START after I ran the 1.10.2 version of patch programmer on a CC3000 with 1.13.
The probIem occurred after the following sequence of ports: First I ported the 1.10.2 version of patch programmer and upgraded my CC3000 that was running version 1.10.1. Then I ported version 1.12 of patch programmer and upgraded the same CC3000 that was now running version 1.10.2. Next I ported version 1.13 of patch programmer and upgraded the firmware of the CC300 that was running version 1.12. After each port, I checked the version with nvmem_read_sp_version to verify that the patch programmer succeeded. Finally I wanted to retry the sequence again, so I downgraded the CC3000 running version 1.13 to 1.10.2 using the exact same compiled image that succeeded the first time. This attempt failed on the driver portion of patch programmer, and I can no longer get any responses to any commands besides the HCI_CMND_SIMPLE_LINK_START.
I have tried re-running each of the patch programmers versions that I have ported and none will work anymore.
Is downgrading not supported with patch programmer? Is there any way that I can recover my corrupted CC3000?
Thank you for your assistance.