Hello all,
We are using the CC3000 with an iOS app which in turn uses the TI's SmartConfig library for the configuration of WiFi parameters on the CC3000. The library is precompiled to 32 bit and within a week, all iOS apps will need to be 64 bit in order to be approved. In another post some users are asking for 64 bit support for the SmartConfig library but without answers from TI. Let's turn the question around, it is possible to use the new WiFi Starter library (already 64 bit) to configure the CC3000? What changes are needed in the app using the library and/or in the CC3000 host code? We tried the WiFi Starter out of the box and it is not working with CC3000.
Regards,
Martin