Helllo All,
One of my customer wants to use CC3000 with STM32F207.
He is having below query. Kindly help to advise.
We had wired TI CC3000MOD with STM32F207 controller and send "HCI_CMND_SIMPLE_LINK_START" command to module through SPI after receiving power on SPI_irq. In response to this command module is not sending reply byte to controller, not even generating SPI_irq.
Even observed Logic level of SPI_out signal, which is between 0 to 1.8V.
Supply voltage for controller and CC3000 module is 3.3V DC. Dose it required any buffer.
Awaiting for your valuable response.