Hi,
I try to interface a cc3000 with my STM32F4. The initialisation is OK, I follow cc3000 Host Programming guide, so I supply the cc3000 at 3.3v with enough power, i put Enable at High State, the IRQ take 60ms to go high and down, and the chip select go down. I done the FirstSpiWrite of 10 bites, the IRQ go high and down after 900 ms. But for the second Write the IRQ is not piloting.
Do you have a solution of my trouble? Do i must put a specific patch programmer on the EPROM device?
Best Regards