First, my apologies posting in what is likly the wrong forum, but I was unable to find a link to creat a new one for this MCU. If you are amoderator, please feel free to move it..
Long tale of woe and frustration.
Several years ago, I started searching for an RF module for a project I had in mind, and for reasons too numerous to list here, I decided there was nothing more ideally suited to my project then the TI CC2511F32, which a company called Pololu had already built into a module they call the Wixel. So I proceeded to do a great deal of development work, both electronic and programming, to build my system which I call "Soundman". It is a general purpose remote control for musicians, "Soundmen", and DJs, permitting them to remotely control multiple audio levels, electric lighting systems (through another module not shown), and guitar/instrument effects. It works great. So great that I have added to the functionality for years now, and would really like to market this thing (and I'd show some photos of the prototypes if anyone is interested.) But now I have a great dilemma, for which I hope you can offer me some better advise then telling me what I already know... that I'm a very stupid person for not taking the time to understand the huge elephant in the air: the FCC.
I knew, and did read in Pololu's literature that they had followed TI's PCB recommendations to the letter, for an antenna made from PC traces, which SHOULD be as acceptable to the FCC as TI says it is. But what I wasn't prepared for was the fact that since this "Wixel" product is NOT certified for modular approval with the FCC, I will probably have to seek FULL FCC approval on my own. Further exploration showed me that this FCC approval was probably going to cost me $10000, maybe double that since two of the devices you see in my photos are being used as transmitters (intentional radiators). Worst, the FCC rules say I'm not allowed to make more than 5 of them without this approval, and am not allowed to sell ANY of them. Wonderful.
So anyway, I'm writing today to seek some advise, and maybe some reason to hope that it doesn't have to be as expensive and forbidding as I think. Perhaps the 2.4Ghz frequency spectrum this TI chip uses, which seems to be designated for "Amateur" usage, might have some relaxed rules that you know of? Or, perhaps some ground work has already been done by TI in the board layout recommendation, that might save me some money.
I am still probably 1/2 year to 1 a year away from having these projects completely finalized, in terms of having manuals and brochures ready. Perhaps I will seek investor funding to help with the FCC situation. But I still will need to know exactly what I'm up against.
I will rant briefly and say that It is a shame that an innovator such as myself should have such a highly useful end product, which possibly will become a dead end that never sees the light of day, because of these steep expenses, while designers in China seem to regularly ship radio controlled toys (similar power output to the TI chip), without any restrictions. All my research is pointing to the fact that I should have started with an approved RF module. Like I said, I already know I'm pretty stupid. I'm just hoping someone at TI, can give me some advise on how to save me from another outright failure. Sorry for my whining... I'm not having a very good day.