I what to verify the specifications for the Analog Temperature Sensor within the CC2543.
In document SWRS107C (April 2012) on page 7 in the section titled "Analog Temperature Sensor", what units are the Temperature Coefficient given in? TYP is 4.5 something per 1 deg-C, is it number of bits out of the 4096 ADC range, or mV's?
I can only find it mentioned only once in another document that the internal band-gap reference for the ADC is 1.15V, would this be the reference voltage used with the 4096 bit combinations to sample the temp sensor?
Ultimately I'm trying to verify the temperature coefficient in mV/deg-C.