Hi all
I just started hacking around with CC3200 launchpad. This board is mostly intended to create wifi enabled equipment . I wonder if I can use the same processor to have in addition an ethernet TCP socket with the proper interfacing logic. Until now i used to connect a wiznet w5200 device interfaced via spi to 8 bit / 16 bit processors to do the job , but since the available libraries for 3200 are huge , i wonder if someone already planned to do somthing like this. The same question i am thinking about possible bluetooth integration with cc3200.
Stefano B.